Electricity is one of the essential utilities in a computing environment. And while the physics of electricity (illuminated by greats like Faraday, Edison, and Tesla) is constant, there’s considerable diversity in how power is transmitted and distributed worldwide.
Take, for example, the deployment of 415 Volt power in North American data centers. In 2023, this isn’t particularly newsworthy. Fifteen years ago, it was novel. Around that time, big data center operators in North America proposed this “international” voltage as an avenue to greater data center efficiency—smaller transformers, fewer losses, and better utilization of power supplies.
Electrical diversity has conditioned us to look at electricity through regional silos. Still today, the prevailing practice is to segment power products according to regional electrical standards and regional conformance bodies like UL & CE. Therefore, any global enterprise likely has unique PDUs for each country/region in which they operate. This leaves a supply chain organization with more to manage—inventory levels, BOMs, configurations—and more opportunity for error.
The Panduit Universal PDU (uPDU) offers an avenue to address PDU deployment challenges.
As soon as a cord/plug is hardwired to a PDU, it becomes regional—the opposite of ‘universal’ and the cause of the supply chain complexities mentioned above. The uPDU is deliberately sold absent a cord and plug and instead offers (12) potential choices called facility side cables.

Consumers will choose the appropriate cable depending on the installation location and capacity required. The two components—PDU and cord—then mate on-site with no required tools.
Part Number
Description
Drop-Down Menu in Web GUI
Apparent Power (kVA)
Input Voltage (V)
Input Phase
UPDUCRD1
UPDU to IEC 60309 3P+N+E 6h 32A (IP44), CORD SET, 3M (10FT)
32A3WYE
"17.3 (NAM)
22.0 (EMEA)"
415
3
UPDUCRD2
UPDU to IEC 60309 2P+E 6h 60A (IP44), CORD SET, 3M (10FT)
"60A1L-L (NAM) 60A1L-N (EMEA)"
10
208
1
UPDUCRD3
UPDU to IEC 60309 3P+E 9h 60A (IP44), CORD SET, 3M (10FT)
60A3DLT
17.3
208
3
UPDUCRD4
UPDU to CS8365C 50A, CORD SET, 3M (10FT)
50A3DLT
14.4
208
3
UPDUCRD5
UPDU to IEC 60309 3P+N+E 6h 63A (IP44), CORD SET, 3M (10FT)
"60A3WYE (NAM) 63A3WYE (EMEA)"
"23.0 (NAM)
27.6 (EMEA) BREAKER LIMITED"
415
3
UPDUCRD6
UPDU to IEC 60309 3P+N+E 6h 20A (IP44), CORD SET, 3M (10FT)
"20A3WYE (NAM) 16A3WYE (EMEA)"
"11.5 (NAM)
11.0 (EMEA)"
415
3
UPDUCRD7
UPDU to L6-30P 30A, CORD SET, 3M (10FT)
30A1L-L
5
208
1
UPDUCRD8
UPDU to IEC 60309 2P+E 6h 20A (IP44), CORD SET, 3M (10FT)
"20A1L-L (NAM) 16A1L-N (EMEA)"
"3.3 (NAM)
3.6 (EMEA)"
240
1
UPDUCRD9
UPDU to IEC 60309 2P+E 6h 32A (IP44), CORD SET, 3M (10FT)
"30A1L-L (NAM) 32A1L-N (EMEA)"
"5.0 (NAM)
7.4 (EMEA)"
240
1
UPDUCRD10
UPDU to L21-30P 30A, CORD SET, 3M (10FT)
30A3WYE
8.6
208
3
UPDUCRD11
UPDU to L15-30P 30A, CORD SET, 3M (10FT)
30A3DLT
8.6
208
3
UPDUCRD12
UPDU to CS8265C 50A, CORD SET, 3M (10FT)
50A1L-L
8.3
208
1
UPDUCRD1
Description
UPDU to IEC 60309 3P+N+E 6h 32A (IP44), CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
32A3WYE
Apparent Power (kVA)
"17.3 (NAM)
22.0 (EMEA)"
Input Voltage (V)
415
Input Phase
3
UPDUCRD2
Description
UPDU to IEC 60309 2P+E 6h 60A (IP44), CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
"60A1L-L (NAM) 60A1L-N (EMEA)"
Apparent Power (kVA)
10
Input Voltage (V)
208
Input Phase
1
UPDUCRD3
Description
UPDU to IEC 60309 3P+E 9h 60A (IP44), CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
60A3DLT
Apparent Power (kVA)
17.3
Input Voltage (V)
208
Input Phase
3
UPDUCRD4
Description
UPDU to CS8365C 50A, CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
50A3DLT
Apparent Power (kVA)
14.4
Input Voltage (V)
208
Input Phase
3
UPDUCRD5
Description
UPDU to IEC 60309 3P+N+E 6h 63A (IP44), CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
"60A3WYE (NAM) 63A3WYE (EMEA)"
Apparent Power (kVA)
"23.0 (NAM)
27.6 (EMEA) BREAKER LIMITED"
Input Voltage (V)
415
Input Phase
3
UPDUCRD6
Description
UPDU to IEC 60309 3P+N+E 6h 20A (IP44), CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
"20A3WYE (NAM) 16A3WYE (EMEA)"
Apparent Power (kVA)
"11.5 (NAM)
11.0 (EMEA)"
Input Voltage (V)
415
Input Phase
3
UPDUCRD7
Description
UPDU to L6-30P 30A, CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
30A1L-L
Apparent Power (kVA)
5
Input Voltage (V)
208
Input Phase
1
UPDUCRD8
Description
UPDU to IEC 60309 2P+E 6h 20A (IP44), CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
"20A1L-L (NAM) 16A1L-N (EMEA)"
Apparent Power (kVA)
"3.3 (NAM)
3.6 (EMEA)"
Input Voltage (V)
240
Input Phase
1
UPDUCRD9
Description
UPDU to IEC 60309 2P+E 6h 32A (IP44), CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
"30A1L-L (NAM) 32A1L-N (EMEA)"
Apparent Power (kVA)
"5.0 (NAM)
7.4 (EMEA)"
Input Voltage (V)
240
Input Phase
1
UPDUCRD10
Description
UPDU to L21-30P 30A, CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
30A3WYE
Apparent Power (kVA)
8.6
Input Voltage (V)
208
Input Phase
3
UPDUCRD11
Description
UPDU to L15-30P 30A, CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
30A3DLT
Apparent Power (kVA)
8.6
Input Voltage (V)
208
Input Phase
3
UPDUCRD12
Description
UPDU to CS8265C 50A, CORD SET, 3M (10FT)
Drop-Down Menu in Web GUI
50A1L-L
Apparent Power (kVA)
8.3
Input Voltage (V)
208
Input Phase
1
* User must select the appropriate drop down from WebGUI menu to achieve stated power metering accuracy.
For a full listing of part numbers including related products, please visit here
The uPDU capacity ranges from 3.3kVA to 27.6 kVA. The internal wiring is sized for the maximum possible current, making it safe to operate at all levels.
Use Cases
Consistency: A user can deploy the same PDU everywhere and stock only the cords needed at each location.
Compliance: Universally compliant PDUs that meet international standards for PDUs[FM3] [RL4]
- USA & Canada: UL/EN/IEC 62368 PDU
- Europe - CE/UKCA Approved
- Australia - RCM Approved
- Brazil: Approved
- Chile: Approved
- Peru: Approved
- United Arab Emirates (UAE): Approved
- India: Approved
- China: Approved
- Hong Kong: Approved
- Singapore: Approved
Adaptability : A recently acquired company faced changing rack power requirements as it had to move its IT gear into the data center of its new owner—one with a completely different power infrastructure. All the existing PDUs had to be scrapped for new models to accommodate these changes. In the same scenario, the uPDU offered a versatile solution, as it could be repurposed in the new environment simply by swapping the facility side cables, thus addressing the altered rack power demands efficiently.
Sustainability: Sustainability is more important than ever. The previous example speaks to it. Traditional rack PDUs may contribute to e-waste when replaced, and new product packaging and transportation can have environmental impacts. Not only do uPDUs keep PDUs from getting scrapped, but data centers save on the packaging and transportation that new products would require.
Summary
The uPDU is a departure from a conventional PDU—not applicable to all consumers but a difference maker for those who operate globally or who have diverse electrical systems to work within.
To learn more about Panduit Critical Power Solutions offering, please visit here.